SF_E_ERR_LED_SETPermalink

This is the web edition of the original ‎⮫ AC500-S safety user manual, version 1.3.2. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements.

04.06.060_SF_E_ERR_LED_SET

Setting E-ERR LED state (ON = TRUE or OFF = FALSE)

E-ERR LED is set directly in the same safety CPU cycle. The state remains unchanged until it is not explicitly changed using SF_E_ERR_LED_SET call.

Table 1134: FUN name: SF_E_ERR_LED_SET

Name

Data type

Initial value

Description, parameter values

VAR_INPUT

SET

BOOL

FALSE

FALSE = E-ERR LED is OFF, TRUE = E-ERR LED is ON

VAR_OUTPUT

SF_E_ERR_LED_SET

BOOL

FALSE

FALSE = E-ERR LED is OFF, TRUE = E-ERR LED is ON

Call in ST

SF_E_ERR_LED_SET_Value := SF_E_ERR_LED_SET(SF_E_ERR_LED_SET_Set);