AddressPermalink

The direct display of individual memory locations is done through the use of special character sequences. These sequences are a concatenation of the percent sign "%", a range prefix, a prefix for the size and one or more natural numbers separated by blank spaces.

Table 1183: Supported range prefixes

I

Input

Q

Output

M

Memory location

Table 1184: Supported size prefixes

X

Single bit

None

Single bit

B

Byte (8 bits)

W

Word (16 bits)

D

Double word (32 bits)

Examples:

%QX7.5 and %Q7.5

Output bit 7.5

%IW215

Input word 215

%QB7

Output byte 7

%MD48

Double word in memory position 48 in the memory location.

%IW2.5.7.1

Depending on the PLC configuration

 ivar AT %IW0 : WORD;

Example of a variable declaration including an address assignment

The current PLC configuration for the program determines whether or not an address is valid.

Boolean values will be allocated bytewise, if no explicit single-bit address is specified.

Example: A change in the value of varbool1 AT %QW0 affects the range from QX0.0 to QX0.7.

Online Change might change the contents on addresses.

Please regard this when using pointer on addresses.

⮫ “Pointer”