This structure contains the following information on the real time given by the local system clock. It is used by the function block CurTimeEx.
|
Component |
Data type |
Description |
|---|---|---|
|
dwLowMSecs |
DWORD |
The value of the real-time clock is returned in microseconds, using a Low DWORD plus a High DWORD, see Structure SysTime64. |
|
dwHighMsec |
DWORD |
|
|
Year |
UINT |
Year, e.g. "2002" |
|
Month |
UINT |
Month, e.g. "12" |
|
Day |
UINT |
Day of month, e.g. "3" |
|
Hour |
UINT |
Hour of the current day, e.g. "13" |
|
Minute |
UINT |
Minutes of the current hour, e.g. "43" |
|
Second |
UINT |
Seconds of the current minute, e.g. "15" |
|
Milliseconds |
UINT |
Milliseconds of the current second, e.g. "649" |
|
DayOfWeek |
UINT |
Day of the week, e.g. "2" (Sunday=0, Monday = 1...) |