SF_WDOG_TIME_SETPermalink

This is the web edition of the original ‎⮫ AC500-S safety user manual, version 1.3.2. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements.

04.06.062_SF_WDOG_TIME_SET

Setting the maximum allowed cycle time of the safety CPU

The SF_WDOG_TIME_SET function block allows the user to monitor the cycle time. The function block must be called by the user during the first cycle. In order to update the outputs ACT_TIME and MAX_TIME, it is necessary to call the function block in each cycle. If the function block is not available in the application, the safety CPU and the application program will enter the SAFE STOP state after the first cycle. The watchdog time is monitored prior to the output of the PROFIsafe telegrams.

If the cycle time is exceeded, an error message is an output and the safety CPU enters the SAFE STOP state. Reasonable values are longer than the typical safety CPU runtime and at least two times shorter than the F_WD_Time of the safety I/O module.

Only one function block instance must be used in the safety program, otherwise a warning is issued.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

The cycle time supervision takes place only in RUN (safety) mode.

Table 1136: FB name: SF_WDOG_TIME_SET

Name

Data type

Initial value

Description, parameter values

VAR_INPUT

EN

BOOL

FALSE

The function block is activated (EN = TRUE) or deactivated (EN = FALSE) via input EN. If the block is active, the current values are available at the outputs.

WDOG

DWORD

16#00000000

Watchdog time in ms. The maximum allowed value is 1000. If WDOG is > 1000, then SAFE STOP state will be entered by the safety CPU.

RESET

BOOL

FALSE

TRUE sets MAX_TIME to 0.

VAR_OUTPUT

DONE

BOOL

FALSE

Output DONE indicates that the set process is finished.

ACT_TIME

DWORD

16#00000000

Actual safety CPU cycle time in ms

MAX_TIME

DWORD

16#00000000

Maximal monitored safety CPU cycle time in ms

Call in ST

SF_WDOG_TIME_SET (EN := SF_WDOG_TIME_SET_EN,
WDOG := SF_WDOG_TIME_SET_WDOG,
RESET := SF_WDOG_TIME_SET_RESET,
DONE => SF_WDOG_TIME_SET_DONE,
ACT_TIME => SF_WDOG_TIME_SET,
MAX_TIME => SF_WDOG_TIME_SET_MAX_TIME);